Map File Name (802.16 OFDMA)
The drop-down list shows the name of the current map file zone definitions. These are the zone definitions that can be applied for analysis when Map File is selected, see Using Map Files.
If there are no map files in the drop-down list, a new one must be created or an existing one imported . To create or import a map file, click button to open the OFDMA Map Files dialog box.
See Also