Map file (Definition Source) (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table.)
Definition Source mode applies a previously stored Map File to the current measurement zone definitions. Map file allows a quick setup, repeat, and/or reproduction of a previous measurement zone definition setup.
Using the Map file Definition Source mode
There must be at least one existing map file loaded to select the Definition Source mode. If there is not an existing map file in the drop-down list, either create or import an existing map file. If there is a Map File, select and then select the name of the map file to use for the measurement from the drop-down list. The selected Map File zone definitions will be immediately applied to the current measurement.
Creating, Importing, and Using Map Files
The button is used to create, edit, delete, export, import or create a Map File from the current measurement setup. Clicking the will open the OFDMA Map Files dialog box, which provides the interface to perform all the Map File functions. To learn about using Map Files, see Using Map Files topic.
The VSA also supports two other zone definition modes; Auto-detect or Manual.
See Also