Detected Allocations (802.16 OFDMA)
trace shows the distributed symbol and subcarrier allocation for each burst defined in the measurement permutation zone. This trace shows the subcarrier to symbol mapping for each burst across the measurement Zone from symbol to symbol.
Interpreting the Detected Allocations trace
The y-axis units represent the tones (or subcarriers) and the x-axis units are the symbol index values. Color is used to identify individual bursts and the subcarrier/symbols that are allocated to that burst. The trace colors are used by other OFDMA traces to identify the common burst information. These OFDMA traces include the Error Vector Time trace, the Error Vector Sprectrum trace, the IQ Meas trace, IQ Ref trace, and the Syms/Errs trace.
Marker Data Results: Symbol Index Number, Name of Burst, Subcarrier Number
See Also
Zone Definition Tab (802.16 OFDMA)
Error Vector Time (802.16 OFDMA)