Statistics Enable (Advanced-Radar/Hopping)

Menu Path: Analysis > Advanced-Radar/Hopping Measurement Properties > Analysis > Statistics Panel

When Statistics Enable is checked (enabled), Pulse Table result metrics from subsequent measurement updates will be included within the accumulated Trend, Histogram and pulse statistical data set.

When Statistics Enable is unchecked (disabled), Pulse Table result metrics from subsequent measurement updates will be excluded from the accumulated Trend, Histogram and pulse statistical data set.

Note that changing the state of the Statistics Enable checkbox while performing continuous measurement updates does not reset the accumulated statistical data set. The accumulated statistical data can be reset by restarting the measurement.

See Also

Remove Mean

Remove Second Order

Remove Slope

Display Length

Internal Buffer Length

Histogram Range Limit