Region Panel (Advanced-Radar/Hopping)

Menu Path: Analysis > Advanced-Radar/Hopping Measurement Properties > Detection

The Region panel is only available when Synchronization Domain is Phase, Frequency or Linear Chirp.

The Region panel provides inputs to configure how regions are detected. The first group of Detection parameters are specific to the selected Synchronization Domain. The Region Detection Filtering parameters are common to Phase, Frequency and Linear Chirp.

Region detection is based on the settling tolerance, as shown in the following diagram:

The Y axes can be Frequency, Frequency Slope, or Phase depending on the synchronization domain.

 

Phase Detection (Synchronization Domain = Phase)

Frequency Detection (Synchronization Domain = Frequency)

Chirp Detection (Synchronization Domain = Linear Chirp)

Region Detection Filtering

See Also

Pulse Panel

Detection Tab

Advanced-Radar/Hopping Measurement Properties Dialog Box