Detection Tab (Advanced-Radar/Hopping)

Menu Path: Analysis > Advanced-Radar/Hopping Measurement Properties > Detection

The Detection tab provides inputs to configure how pulses, chirps and regions are detected. The available detection panels and parameters depend on the selected synchronization domain.

Synchronization Domain -- This parameter is provided on every tab because it is a fundamental configuration parameter affecting the entire Advanced-Radar/Hopping measurement.

____________________________________________

Detection parameters are grouped into the following panels:

See Also

Advanced-Radar/Hopping Measurement Properties Dialog Box