Pulse Panel (Advanced-Radar/Hopping)

Menu Path: Analysis > Advanced-Radar/Hopping Measurement Properties > Detection

The Pulse panel is available when Synchronization Domain is either Amplitude (Pulsed) or Linear Chirp with the Pulsed checkbox selected.

The Pulse panel provides inputs to configure how unique pulses are detected in the Synchronization Domain.

If the noise floor of your signal is particularly high, this could interfere with the calculation of the Top/Base of the pulse, and thus interfere with the detection of the pulse. Consider using a Top/Base Calculation Method of Mean to compensate for this. This setting can be found on the Calculation tab under the Metric Calculation Thresholds grouping.

 

The following pulse detection parameters are available:

Optional Detection Filtering

See Also

Region Panel

Detection Tab

Advanced-Radar/Hopping Measurement Properties Dialog Box