Component Test Properties Dialog Box

The Component Test Properties dialog box contains parameters for configuring a component test measurement.

Component Test must be selected before this dialog box is available. Click Analysis > Measurement Type > General Purpose > Component Test.

The Closed tabbed dialog box contains the following property groups:

Component Test Properties can also be viewed as a Closed tabless dialog box (with accordion-style drop-downs) by toggling the Use tabbed dialog button .

See Also

Selecting the Component Test Measurement Type

Making a Component Test Measurement