Load Ref Data IQ values (CCn) (CustomOFDM)
The button opens a dialog to load a "*.csv" formatted text file that contains an array of reference data (refData) in-phase/quadrature (IQ) values. The Values are loaded into the Reference Data IQ Values parameter text box.
If the data in the data IQ values array is insufficient to populate the resource map, the data IQ values are repeated to fill the remaining resource map data locations.
Load Ref Data IQ Values acts on the component carrier scope chosen with the Component Carrier control at the top of the tab. The button caption shows the scope it will act on:
-
Load Ref Data IQ Values (CCn) — an individual component carrier is selected, and only that carrier is configured. The other component carriers are unchanged.
-
Load Ref Data IQ Values (All CC) — all component carriers are selected, and every component carrier is configured.
See Also