Reference Preamble IQ Values (Custom OFDM)
The parameter specifies the reference values of the preamble subcarriers. Each preamble subcarrier is represented by a complex value, "I" the Real part followed by "Q" the Imaginary part, that is repeated for each subcarrier.
Reference Preamble I-Q File
The Preamble I-Q file The Preamble I-Q file defines the expected I and Q values for each preamble subcarrier. defines the expected I and Q values for each preamble subcarrier. This file contains I and Q values for every preamble subcarrier (Resource Type Resurce Type specifies the function of the measurement subcarriers; preamble, pilot, data, All, UserN, Unknown, or Null subcarrier 3) defined in the Resource Map file The Resource Map file defines the function of each subcarrier in each symbol, describing whether it is a preamble, pilot, data or null subcarrier.. Each time the demodulator encounters a “3” in the Resource Map file, it reads the next two values from the Preamble I-Q file and uses these values as the ideal I-Q location for that preamble subcarrier.
For more information, see "Preamble I-Q File" in the Making a Custom OFDM Measurement tutorial.
See Also