Load Ref Pilot IQ Values (CCn) (Custom OFDM)
The button opens a dialog to load a "*.csv" formatted text file that contains an array of the Pilot I and Q reference values for each Pilot Subcarrier. The Values are loaded into the Reference Pilot IQ Values parameter text box.
If the number of pilots in the pilot IQ values array is insufficient to populate the resource map, the pilot IQ values are repeated to fill the remaining resource map pilot locations.
Load Ref Pilot IQ Values acts on the component carrier scope chosen with the Component Carrier control at the top of the tab. The button caption shows the scope it will act on:
-
Load Ref Pilot IQ Values (CCn) — an individual component carrier is selected, and only that carrier is configured. The other component carriers are unchanged.
-
Load Ref Pilot IQ Values (All CC) — all component carriers are selected, and every component carrier is configured.
See Also