Reference Pilot IQ Values (Custom OFDM)
The parameter specifies the reference values of the pilot subcarriers. Each Pilot subcarrier is represented by a complex value, "I" the Real part followed by "Q" the Imaginary part, that is repeated for each subcarrier.
Reference Pilot I-Q File
You can create a reusable Pilot IQ values file. The Pilot I-Q file The Pilot I-Q file defines the expected I and Q values for each pilot subcarrier. contains the ideal I-Q locations for each known pilot (resource type = 1) shown in the Resource Map file The Resource Map file defines the function of each subcarrier in each symbol, describing whether it is a preamble, pilot, data or null subcarrier..
For more information, see "Reference Pilot I-Q File" in the Making a Custom OFDM Measurement tutorial.
See Also