Load Ref Preamble IQ values (CCn) (CustomOFDM)

The Load Ref Preamble IQ Values (CCn)... button opens a dialog to load a "*.csv" formatted text file that contains an array of the Preamble I and Q reference values for each Preamble Subcarrier.  The Values are loaded into the Reference Preamble IQ Values parameter text box.

If the number of preambles in the preamble IQ values array is insufficient to populate the resource map, the preamble IQ values are repeated to fill the remaining resource map preamble locations.

Load Ref Preamble IQ Values acts on the component carrier scope chosen with the Component Carrier control at the top of the tab. The button caption shows the scope it will act on:

See Also

Format tab

Custom OFDM Demod Properties