Synchronization Antenna Port (Custom OFDM)
0
sets the index of antenna port which is used for synchronization. For MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. measurement, there may be multiple preambles or pilots transmitted on multiple (virtual) antenna ports, and they are used for channel estimation for that antenna port. This value indicates on which antenna port, the corresponding preamble or pilot will be searched for the initial synchronization on the input channel defined by the Synchronization Channel Index parameter. Synchronization Antenna Port and Synchronization Channel Index are also used to decide the relative reference path used in the OFDM MIMO Info table's Phase Offset and TAE metrics.
See Also