Synchronization Channel Index (Custom OFDM)
0
sets the index of the input channel which is used for synchronization. For MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. measurement, there may be multiple preambles or pilots transmitted on different input channels. This value indicates on which input channel the preamble or pilot defined by Synchronization Antenna Port should be searched for the initial synchronization. Synchronization Channel Index and Synchronization Antenna Port are also used to decide the relative reference path used in the OFDM MIMO Info table's Phase Offset and TAE metrics.
See Also