Resource Allocation Diagram (Custom OFDM)
Menu Path:
The
displays a color-coded visual representation of the resource allocations. The legend to the right of the diagram shows the color coding of the Data, Pilot, Preamble and Idle parts of the frame. Hovering over the diagram will display a tooltip with Subcarrier Index, Symbol Index, User ID and Channel Type information at the cursor location.
The Resource Allocation Diagram is also displayed on the Frame Definition tab.
See Also