Time Gaps (Custom OFDM)
Menu Path:
Default: empty array (no gaps in signal)
Time Gaps sets an array of gaps between symbols. Some OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. signal formats may have empty gaps or other non-OFDM signal content between OFDM symbols. Time Gap allows for proper demodulation of these signals.
The Time Gaps property is an array, with one value for each symbol in the signal. Each value specifies the number of samples of time gap, at the OFDM system sample frequency, at the start of the OFDM symbol.
See Also