Time Gaps Repeat Index (Custom OFDM)
Menu Path:
Default: 0
Time Gaps Repeat Index - If the Time Gaps array is at least as long as the measurement result length, it provides a time gap value for each symbol. If the array is shorter than the measurement result length, processing loops back and re-uses the array (and keeps looping back every time the end of the array is reached again). The location within the array that is looped back to is determined by the Time Gaps Repeat Index. This repeat index works the same way as the Guard Interval Repeat Index works with the Guard Interval Per Symbol array.
See Also