Transmitter Window Beta (Custom OFDM)
: SeeThe OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. FFT Fast Fourier Transform: A mathematical operation performed on a time-domain signal to yield the individual spectral components that constitute the signal. See Spectrum. length (unless value).
parameter species the window filter Beta value. Beta is the amount of windowing used by the transmitter to smooth the transition between symbols. Beta is specified as a fraction of theSee Also