Allocation Summary (Custom OFDM)
The Allocation Summary grid lists details about the configured frame allocations.
indicates the priority of the allocation. Lower numbers indicate higher priority (0 is highest). You can adjust the priority of an allocation by clicking one of the Move buttons to the right of the Allocation Summary list.
enables or disables the analysis of an allocation. At least one is always enabled. If you try to disable all of them, the first allocation will be automatically enabled. This setting is editable from the Allocation Summary list or from the allocation's Configuration parameter group.
Default: Enabled
indicates the Name assigned to the this allocation's frame part.
indicates the Name assigned to this allocation.
Indicates User Name assigned to this allocation for the purpose of results reporting (and combining of results of multiple allocations) within the OFDM Data Burst Info results trace.
Indicates allocation Type. This setting is editable from the Allocation Summary list or from the allocation's Configuration parameter group.
indicates the allocation's Power Boost level. This setting is editable from the Allocation Summary list or from the allocation's Configuration parameter group.
indicates the allocation's Payload Sequence. This setting is editable from the Allocation Summary list or from the allocation's Configuration parameter group.
(if Sequence for this allocation is set to Custom) indicates the allocation's Payload Custom Sequence. This setting is editable from the Allocation Summary list or from the allocation's Configuration parameter group.
Indicates the allocation's Modulation format. This setting is editable from the Allocation Summary list or from the allocation's Configuration parameter group.
Indicates the allocation's Active Symbols. This setting is editable from the Allocation Summary list or from the allocation's Configuration parameter group.
Indicates the allocation's Active Subcarriers. This setting is editable from the Allocation Summary list or from the allocation's Configuration parameter group.
Indicates the allocation's Active Port (Pilot or Preamble Type) or Active Ports (Data or Idle Type). This setting is editable from the Allocation Summary list or from the allocation's Configuration parameter group.
See Also