Allocation Parameters (Custom OFDM)
Configuration
Configuration contains parameters that specify the allocation's name, user name, type, power boost and payload.
enables or disables the analysis of an allocation. At least one is always enabled. If you try to disable all of them, the first allocation will be automatically enabled.
sets name of the selected allocation (limited to 30 characters).
sets the associated User Name assigned to this Allocation for the purpose of results reporting within the OFDM Data Burst Info results trace.
If (User Name) Auto is set to false, the User Name value can be manually set. By manually setting multiple allocations within a given frame part to share the same User Name value, it is possible to combine the measured EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format., Power, Modulation Format and Resource Unit metrics of those allocations into a single reported User Name results row within the OFDM Data Burst Info results trace.
If (User Name) Auto is set to true (default), the User Name string value is automatically set equal to the allocations unique Name, supporting separate per allocation result row reporting of EVM, Power, Modulation Format and Resource Unit metrics within the OFDM Data Burst Info results trace.
selects the allocation type. The allocation type is also selectable in the Type column of the Allocation Summary.
- Preamble- configures the allocation as a preamble. Preamble allocations are used for initial sync and channel estimation.
- Data- configures the allocation as data. Data allocations carry data payload.
- Pilot- configures the allocation as a pilot. Pilot allocations are typically interspersed within the data and are used for tracking and updating channel estimation.
- Idle- configures the allocation as idle. Idle allocations are the off, or ignored, portion of the frame.
Default: Data
Range: Preamble, Data, Pilot, Idle
sets the relative power boosting (dB) of this allocation relative to the other allocations.
All constellations are normalized to the same RMS power, so absolute power of the 0 dB level is set to the measured RMS average of all allocations whose PowerBoostLevel is 0 dB.
Default: 0
Payload
specifies the allocation's PN 1) part number, or 2) packet number sequence.
- Unknown - specifies that the payload is unknown (known modulation). Only Unknown is supported for Data allocations.
- PN9 - specifies a PN9 bit sequence, as specified in CCITT T-REC-O.153.
- PN11 - specifies a PN11 bit sequence, as specified in CCITT T-REC-O.153.
- PN15 - specifies a PN15 bit sequence, as specified in CCITT T-REC-O.151.
- PN20 - specifies a PN20 bit sequence, as specified in CCITT T-REC-O.153.
- PN23 - specifies a PN23 bit sequence, as specified in CCITT T-REC-O.151.
- Custom - specifies a custom sequence.
Default: PN23
(only supported for Preamble/Pilots) specifies the type of custom sequence when Sequence is set to Custom. After selecting the Custom Sequence Type, enter or paste the sequence into the field below the Modulation parameter, making sure the entered data matches the specified type. Custom sequences are loaded onto the subcarriers starting with the lowest subcarrier and continuing to the highest subcarrier, then to the next symbol starting at the lowest subcarrier, etc.
Bit Sequence- Bit Sequence is a list of digits (0 or 1) that can be separated by comma, NewLine or no space.
BPSK Binary phase shift keying - A type of phase modulation using 2 distinct carrier phases to signal ones and zeros. mapping table:
Symbol Index BPSK Symbol (I, Q) Bits 0 (1.0, 0) 0 1 (-1.0, 0) 1 QPSK Quadrature phase shift keying mapping table:
Symbol Index QPSK Symbol (I, Q) Bits (MSB Most significant bit. In a binary coding scheme, the bit having the greatest numerical value. Analogous to the left-most numeric position in a decimal number., LSB Least Significant Bit: In a binary coding scheme, the bit having the least numerical value. Analogous to the units position in a decimal number.) 0 (0.707,0.707) (0,0) 1 (-0.707,0.707) (0,1) 2 (0.707, -0.707) (1,0) 3 (-0.707,-0.707) (1,1) Example:
If the bit sequence in the file is: 001011101011…
- For BPSK, bits are mapped to symbol indexes: 0, 0, 1, 0, 1, 1, 1, 0, 1, 0, 1, 1, …
- For QPSK, bits are separated into groups 00,10,11,10,10,11, and they are mapped to symbol indexes: 0, 2, 3, 2, 2, 3, ...
Example .txt files containing the VSA CustomOFDM modulation symbol to bit mappings are installed with the VSA software in the following default directory path:
%PROGRAMFILES%\Keysight\89600 Software <ReleaseVersion>\89600 VSA Software\Help\Signals\Custom OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS.\ConstellationMappings\
IQ Symbol Sequence- IQ Symbol Sequence is a comma or NewLine separated list of interleaved real and imaginary values, representing the IQ symbols in the allocation payload.
selects the allocation's modulation format. The modulation is also selectable in the Modulation column of the Allocation Summary.
- Unknown - the allocation's modulation format is unknown and autodetection will be attempted.
- BPSK- the allocation uses a BPSK modulation format.
- QPSK- the allocation uses a QPSK modulation format.
- 8-PSK Phase Shift Keying: A broad classification of modulation techniques where the information to be transmitted is contained in the phase of the carrier wave.- (data allocations only) the allocation uses an 8-PSK modulation format.
- 16-QAM Quadrature Amplitude Modulation- (data allocations only) the allocation uses a 16-QAM modulation format.
- 32-QAM- (data allocations only) the allocation uses a 32-QAM modulation format.
- 64-QAM- (data allocations only) the allocation uses a 64-QAM modulation format.
- 128-QAM- (data allocations only) the allocation uses a 128-QAM modulation format.
- 256-QAM- (data allocations only) the allocation uses a 256-QAM modulation format.
- 512-QAM- (data allocations only) the allocation uses a 512-QAM modulation format.
- 1024-QAM- (data allocations only) the allocation uses a 1024-QAM modulation format.
- 2048-QAM- (data allocations only) the allocation uses a 2048-QAM modulation format.
- 4096-QAM- (data allocations only) the allocation uses a 4096-QAM modulation format.
- 8192-QAM- (data allocations only) the allocation uses a 8192-QAM modulation format.
- 16384-QAM- (data allocations only) the allocation uses a 16384-QAM modulation format.
- Custom- Uses symbol and I/Q pairs from a user-defined custom modulation definition (see Custom Modulation tab) as the reference constellation for EVM analysis of this allocation.
Default: BPSK
(only visible when Modulation is set to Custom) drop-down list of all custom modulation names currently defined in the Custom Modulation library. Select the definition to use for this allocation's EVM reference.
(only visible when Modulation is set to Custom) shortcut button that opens the Import Custom Modulation Constellation dialog, allowing a new definition to be imported without navigating to the Custom Modulation tab.
Location
Location contains parameters that specify the size and location of each allocation within the frame.
sets the active symbol index(es) for this allocation. The active symbols are also shown in the Symbols column of the Allocation Summary. Use commas to separate individual symbols and colons to define a range of ODFM symbols. Supports colon range notation: start:stop (e.g., 0:5 = symbols 0–5) and start:step:stop (e.g., 0:2:6 = 0, 2, 4, 6). When multiple symbol/subcarrier blocks are configured, this field is read-only and displays all blocks in grouped format: {0|spec},{1|spec},..., where each token shows the group index and its range spec (e.g., {0|0:2},{1|4:5}).
When exactly one block is defined (default), Active Symbols is editable directly. When two or more blocks are configured, this field becomes read-only and displays the grouped spec; the block definitions are managed exclusively through the Symbol Subcarrier Configuration dialog.
Example: 0,2,10:13
Default: 0
sets the active subcarrier index(es) for this allocation. The active subcarriers are also shown in the Subcarriers column of the Allocation Summary. Use commas to separate individual subcarriers and colons to define a range of subcarriers.
When exactly one block is defined (default), Active Subcarriers is editable directly. When two or more blocks are configured, this field becomes read-only and displays the grouped spec; the block definitions are managed exclusively through the Symbol Subcarrier Configuration dialog.
Example: 0,2,5:7
Default: 0
opens the Symbol Subcarrier Configuration dialog. Use this button to define two or more independent symbol/subcarrier groups within the same allocation.
MIMO Configuration
MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. Configuration contains parameters that specify the allocation's antenna port mapping definitions.
(Allocation Type set to either Pilot or Preamble) - Specifies a single antenna port index to which the allocation is mapped.
Range: 0 to (Transmitter Antennas - 1)
(Allocation Type set to either Data or Idle) - Specifies the indexes of the active antenna port(s) that are mapped to the allocation. Enter the port indexes as a comma-separated list. Use a colon (:) to indicate a range of ports.
Range: 0 to (Transmitter Antennas - 1)
See Also