Frame Diagram (Custom OFDM)

Analysis > Custom OFDM Demod Properties > Format tab

The Frame Diagram displays a color-coded visual representation of the frame's resource allocations. The legend to the right of the diagram shows the color coding of the Data, Pilot, Preamble and Idle parts of the frame. Hovering over the diagram will display a tooltip with Subcarrier Index, Symbol Index, User ID and Channel Type information at the cursor location.

The Frame Diagram is displayed on the Frame Definition and Format tabs.

See Also

Frame Definition Tab

Format Tab

Custom OFDM Demod Properties