Frame Parts Editor (Custom OFDM)
Frame Parts is an editor that lets you assemble frame parts and allocations to demodulate and analyze custom signals.
The main Frame Parts panel consists of a default frame part (FramePart0) with a single allocation (Alloc0). Clicking a frame part will display Frame Part Parameters to configure the selected frame. Clicking an allocation will display Allocation Parameters to configure the selected allocation.
Use the following basic frame building tools to create the structure of the desired signal:
Adds a frame part to the list of frame parts and allocations.
Removes the selected frame part from the list of frame parts.
Adds an allocation to the selected frame part.
Removes the selected allocation from the list of frame parts and allocations.
See Also