Location (Custom OFDM)
Location contains parameters that specify the size and location of each allocation within the frame.
sets the active symbol index(es) for this allocation. The active symbols are also shown in the Symbols column of the Allocation Summary. Use commas to separate individual symbols and colons to define a range of symbols.
Example: 0,2,10:13
Default: <blank>
sets the active subcarrier index(es) for this allocation. The active subcarriers are also shown in the Subcarriers column of the Allocation Summary. Use commas to separate individual subcarriers and colons to define a range of subcarriers.
Example: 0,2,5:7
Default: <blank>
See Also