Symbol Subcarrier Configuration Dialog (Custom OFDM)

Use the Symbol Subcarrier Configuration dialog to define two or more independent symbol/subcarrier groups within the same allocation.

Count sets the number of symbol/subcarrier blocks (groups) for this allocation. Increasing the count adds blank rows to the table; decreasing removes rows from the bottom.

Symbols is a comma-separated list of OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. symbol indexes for this block. Supports colon range notation: start:stop or start:step:stop.

Subcarriers is a comma-separated list of subcarrier indexes for this block. Supports colon range notation: start:stop or start:step:stop.

Cancel validates and commits all block definitions to the allocation. An error dialog is shown if any block contains empty or invalid values.

Apply closes the dialog without applying changes.

See Also

Allocation Parameters

Frame Definition Tab

Custom OFDM Properties Dialog Box