Troubleshooting (Digital Demodulation)
This topic contains information to help troubleshoot measurements when using Digital Demodulation. Also see Setting up a Digital Demod Measurement for additional measurement information.
In VSA version 20.00, the default values when first selecting the Digital Demodulation measurement type were changed for the following settings:
- Changed from 24.3 kHz kiloHertz: A radio frequency measurement (one kilohertz = one thousand cycles per second). to Frequency Span/2.
- Changed from ON (selected) to OFF (cleared).
If you use the previous default values for existing measurements, you may get unexpected results unless you change manually these settings to their previous values.
|
PROBLEM |
POSSIBLE CAUSE |
SOLUTION |
|---|---|---|
|
Demodulation fails to lock on signal |
Signal not present |
Check connections |
|
|
Carrier too far from center frequency |
Adjust frequency |
|
|
Input is over-loaded or under ranged |
Adjust input |
|
|
Frequency span is too narrow |
Increase frequency |
|
|
Signal is pulsed |
Set ON |
|
|
Signal is pulsed and result length is longer than pulse |
Decrease . |
|
|
Signal is too noisy |
Try selecting the Low SNR Enhancement checkbox (Advanced Tab of Demod Properties). Must be in a modulation format that supports Low SNR Signal-to-Noise Ratio Enhancement. |
|
|
Wrong symbol rate |
Enter correct (not bit rate) |
|
|
Wrong filter selections |
Select proper measurement and reference filters and correct setting for Alpha / BT. |
|
|
Wrong modulation format |
Select correct modulation format |
|
|
I/Q offset too large |
Reduce LO feedthrough (or DC offset for I+jQ receiver) |
|
|
I/Q misaligned using I+jQ receiver |
Ensure that ch1 and ch2 trigger delays are correct |
|
Spectrum Disappears |
Spectrum not present or digital demodulation not configured correctly. |
View the trace (Trace > Data > Spectrum). If Pulse Search is on also examine the time and search time traces (Trace > Data > Time or Trace > Data > Search Time). Use these traces to determine if the spectrum is present or if the digital demodulator isn't configured properly. |
|
|
|
|
|
Eye diagrams show incorrect symbol timing |
Signal path has phase distortion |
Adjust clock delay to minimize EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. |
|
|
Clock delay is incorrect |
Adjust clock delay to minimize EVM |
|
|
I and Q are misaligned using I+jQ receiver |
Check trigger delay and cable length Adjust for delay using external calibration |
|
|
Signal path limits amplitude fluctuations for non-MSK Minimum Shift Keying signals |
Remove non-linearity, or compensate with clock delay |
|
|
|
|
|
SYNC NOT FOUND |
Search length too short or search offset incorrect |
Increase , adjust search offset |
|
|
Incorrect sync word |
Check and correct sync word |
|
|
Incorrect state definitions |
Change state definitions or sync word |
|
|
Wrong MSK demodulator |
Select correct MSK demodulator |
|
|
|
|
|
PULSE NOT FOUND |
Signal not pulsed |
Turn off |
|
|
Search length too short |
Increase or adjust triggering to ensure that leading and trailing edges of pulse are fully within search length |
|
|
Signal length not optimized |
Try the following method to determine when performing a Pulse Search: SL = (2*MaxOn) + MaxOff Where:SL is search length in seconds. MaxOn is the maximum on time of a pulse in seconds. MaxOff is the maximum off time between pulses in seconds. |
|
|
|
|
|
Pulse found but incorrectly aligned |
Poor signal-to noise ratio or on/off ratio |
Check input setting Reduce to eliminate excess noise and interfering signals. |
|
|
Pulse is asymmetrical |
Use Constellation Sync Search to align result length |
|
|
Span is too narrow |
Increase to prevent degradation of pulse edges |
|
|
|
|
|
Error Vector Time shows large error between symbols |
Wrong filter alpha |
Adjust filter's |
|
|
|
|
|
Error Vector Time shows regions of large errors |
Distortion or a poor signal to-noise ratio causing bit errors |
Check input |
|
|
Large frequency errors interfering with carrier lock |
Adjust frequency |
|
|
Large I/Q offsets causing bit errors |
Reduce LO feedthrough (or DC offset if using I+jQ receiver) |
|
|
|
|
|
EVM larger than expected and Error Vector Time shows errors that increase towards beginning and end of result length |
Wrong symbol rate |
Make fine adjustments to the |
|
|
Result length larger than pulse |
Decrease |
|
|
|
|
|
EVM larger than expected and Error Vector Time shows a uniform distribution of errors |
Frequency span too narrow |
Increase |
|
|
Input is overloaded or under ranged |
Adjust input |
|
|
Result length is too short |
Increase result length |
|
|
Wrong filter selections |
Check that filter selections allow the filtered measured signal to match the reference signal |
|
|
Channel conditions have biased symbol timing recovery |
Observe eye diagrams and adjust clock delay to compensate symbol timing recovery. |
|
|
Time corrections disabled |
Enable time corrections |
|
|
Signal too close to DC |
Increase carrier frequency |
|
|
I and Q misaligned using I+jQ receiver |
Check trigger delay settings and cable lengths |
|
|
AC coupling when using I+jQ receiver |
Select on both input channels |
|
|
I and Q imbalance |
Ensure impedance is identical for both inputs |
|
|
Sync enabled and sync word not unique. Result incorrectly positioned with respect to signal |
Ensure that sync word is unique |
|
|
For MSK type 1, signal contains I/Q offset |
Select to remove I/Q offset term from result |
|
The trace data constellation symbol location shape, such as dots, is not properly displayed. |
The display driver is not functioning correctly. |
Contact your PC manufacturer to see if a newer version of the display driver is available. If not, try decreasing the hardware acceleration. See the Windows documentation for instructions. |
See Also
Parameter Interactions (Digital Demod)