TSC (GSM/EDGE/EDGE Evolution)
TSCdisplays the training sequence code index(es) for the demodulated burst (determined by the Timeslot parameter). The TSC is autodetected when TSC Index is set to .
For modulation, TSCdisplays two values. Each value is of the form SetX-n, where X is the set number and n is the TSC index in that set. Subchannel A uses TSC values from Set 1 and Subchannel B uses values from Set 1 or Set 2.
Programmatically Querying the Summary Table
When querying the through the VSA API 1) Access Preamble Indicator, or 2) Application Programming Interface, the value for the TSC metric for modulation is in the following form:
AaaBbb
where A and B are the TSC sets for subchannels A and B, respectively
aa and bb are the TSC codes within the sets for subchannels A and B, respectively
For other modulation types, the value for TSC is a single number.
See Also