Frame Configuration (Flex Frame)

Frame Configuration is a sub-tab of the Component Carrier Configuration parameter group, and contains parameters that apply to all allocations within the frame.

Frame Type determines how the demodulator searches for the beginning of the frame. It also affects parameters such as Search Length and Result Length.

Default: Burst

Choices: Burst, Periodic

Symbol Rate sets the frame symbol rate in Hz.

Default: Depends on the Current Analyzer Configuration

Symbol Rate and the measurement Span are linked. When you change Symbol Rate, the span is adjusted automatically to suit it: the span is held to no more than 10 times the signal bandwidth - which is the symbol rate itself for a single carrier, or the total occupied bandwidth when carriers are aggregated - and to no less than 1/100 of the symbol rate. You do not normally need to set Span before setting Symbol Rate.

Length sets the length of the frame in number of symbols.

When Frame Type is set to Burst, an Auto checkbox is available that, when selected, automatically sets the frame length based on the detected burst length.

Default: 1000 symbols

See Also

Measurement Control Tab

Component Carrier Configuration

Scrambling