Measurement Control Tab (Flex Frame - Advanced Mode)
The tab of the configures the Flex Frame measurement characteristics.
The measurement control settings are applied to either a single carrier or to all carriers, depending on the Component Carrier Selection. Use the Component Carrier drop-down or the Component Carrier Diagram at the top of the tab to switch between component carriers.
The Measurement Control tab configures these parameters:
Frequency Estimation & Equalization & Synchronization
- Synchronization Source
- Frequency Estimation Mode
- Equalization Mode
- Cost Function Criteria
- Channel Estimation Source
- Initial Equalization
- Normalized Channel Delay Spread
- EQ Tracking
- Tracking Convergence
See Also
Flex Frame Properties Dialog Box