Frame Parts (Flex Frame)
Frame Parts is an editor that lets you assemble frame parts and allocations to demodulate and analyze custom signals.
The main Frame Parts panel consists of a default frame part (FramePart0) with a single allocation (Alloc0). Clicking the allocation will display a Configuration property panel to specify the allocation's name, type, power boost and payload, and a Location property panel to specify the length, location and repetition of symbols per allocation within the frame.
Use the following basic frame building tools to create the structure of the desired signal:
Adds a frame part to the list of frame parts and allocations.
Removes the selected frame part from the list of frame parts.
Adds an allocation to the selected frame part.
Removes the selected allocation from the list of frame parts and allocations.
sets the name of the frame part.
See Also