About Default Bit Mappings (Flex Frame)
When you set to , the VSA uses non-standard-specific bit mapping. The VSA software includes mapping files for each Modulation type, which you can recall in Keysight N7608C Signal Studio Pro for Custom Modulation to make sure your created signals have the appropriate constellation mapping. These files are located in the following default installation directory:
%PROGRAMFILES%\Keysight\89600 Software <ReleaseVersion>\89600 VSA Software\Help\Signals\FlexFrame
The FlexFrame folder also contains .txt files without "Default" in the name, which can imported in VSA and Signal Studio when using Custom Modulations.
Installed Default Bit Mapping Files
- BPSK_Default.txt
- QPSK_Default.txt
- 8PSK_Default.txt
- 16QAM_Default.txt
- 64QAM_Default.txt
- 256QAM_Default.txt
- 1024QAM_Default.txt
BPSK_Default.txt
QPSK_Default.txt
8PSK_Default.txt
16QAM_Default.txt
64QAM_Default.txt
256QAM_Default.txt
1024QAM_Default.txt
See Also