Selecting Flex Frame

Menu Path: Analysis > Type > Flex Frame

Selecting the Flex Frame measurement type configures the VSA to use a flexible frame manager to measure EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. in custom signals.

Example recordings

The 89600 VSA includes several example signals that can be used to help you learn how to use Flex Frame. The included signals are listed in the Demo and Recorded Signals topic in the Getting Started book. Specifically, see the signals in the FlexFrame folder.

See Also

Flex Frame Properties Dialog Box

About Flex Frame