Time Tab (Flex Frame - Basic Mode)
The (Basic Mode) tab sets how much data to acquire for the frame.
defines the number of symbols used to compute measurement results shown in the IQ traces, Error traces, and Time trace.
when checked, specifies that the demod should do a burst search to find the transmitted symbols. When unchecked, no burst search is performed and the data is assumed to be continuously transmitted symbols. See Pulse Search (Digital Demod) for more information.
- determines how much total data to acquire in order to do pulse search. See Pulse Search (Digital Demod) for more information.
when checked, will cause a second allocation (Sync) to be defined in the frame. The bit pattern to search for can be entered in the Bit Pattern field.
- provides a space to enter a (binary) bit pattern to search for. The bits are mapped to the symbols using the Default Bit Mappings.
- sets the location of the sync relative to the start of the frame, in symbols.
See Also
Flex Frame Properties Dialog Box