Phase Trace Data
The Phase Trace results include:
- Inst Phase Error
A non-averaged version of Phase Error Time.
- Inst Phase Meas
A non-averaged version of Phase Meas Time.
- Phase Error
Reports region-synchronized measured signal phase error samples over time in degree. [i.e. Phase Error Time = Phase Meas Time - Phase Ref Time].
- Phase Meas
Reports region-synchronized measured signal phase samples over time in degree.
- Phase Ref
Reports region-synchronized reference signal phase samples over time in degree.
Note that Selected Regions affects which pulses are displayed in the Amplitude, Phase, and FM Frequency Modulation traces.
See Also