Result Tables
Menu Path:
The FMCW Radar Measurement allows you to display tables that list reported performance metrics for each detected LFM Region within the current acquisition. See the Matrix Tables reference topic for more information.
You can select from the following table formats.
-
Region Table – displays a list of reported performance metric for each detected region within the current Acquisition.
-
Cumulative Stats – displays accumulated statistics of each reported performance metric based on all detected regions since last Measurement Restart event (includes current plus previous acquisitions). The number of regions listed is the number of complete regions.
-
Current Stats – displays Min, Max, Avg, Std Dev of each reported performance metric based on the set of detected regions within the current Acquisition.
-
Summary - displays Average Power, Peak Power, Detection Threshold, Top Level, Base Level, Top/Base and Time Offset for the current acquisition.
-
CCDF Summary - displays CCDF Complementary Cumulative Distribution Function power data.
Cumulative statistics are reset whenever the measurement is restarted. They are not reset when the measurement is paused.
FMCW Statistics
Statistics are derived from the current stream of regions. Each measurement is considered a new group of data. For example, if there are four regions in a measurement, then the statistical parameters of the four regions are calculated. The maximum of the four regions is computed and listed as the maximum.
Statistics are calculated for each parameter. For example, if there are four regions , then Max will be the maximum rise time for the four regions . Similarly, Min is the minimum rise time for the four regions:
Statistics are divided into two groups:
- Statistics for the current regions, and
- Cumulative statistics gathered since the last measurement restart. Trend analysis can be enabled or disabled without resetting the measurement.
The statistics captured are:
-
max -- maximum value for given parameter in region stream
-
min -- minimum value for given parameter in region stream
-
average -- average of given parameter for all of the regions
- rms -- root of the mean of the squares of given parameter for all of the regions
-
std dev -- standard deviation of given parameter for all of the regions
The statistics are calculated based on the underlying units in the Region Table, so values that are expressed in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer are averaged in dBm instead of translating to Watts first.
The statistics tables also contain a Count row, which indicates the number of points included for each metric. There is no separate Count row for Median and Mode since the Count row is accurate for those metrics until the number of points in the Count row is greater than the trend buffer length, at which time the count for Mode and Median is the trend buffer length.
See Also