Current Stats Table
Menu Path:
The Current Stats table is a type of Matrix Table that reports the following statistical information for each reported Region Table performance metric, based on the set of detected LFM regions detected within the current Acquisition Length (s), up to the specified Maximum Region Count value.
- Minimum
- Maximum
- RMS
- Average
- Std Dev (Standard Deviation)
- Count (reports statistical data set count of detected LFM regions within the current acquisition)
Reference Region Count describes the number of unique LFM regions contained within each repetition instance of the measured signal's LFM region-group pattern. This value is used for Ref Region identification within FMCW Region Table results, plus associated per Ref Region statistical metric reporting within Current Record Statistics and Cumulative Statistics.
The illustration below shows an example of the Current Record Statistics table metrics that are displayed after a Preset Columns operation (right-click any column, then click Preset Columns):