Available Trace Formats
All trace formats are available for all options of the VSA, but some are only applicable to demod options (like Constellation and Q-Eye). A trace format can be selected from the dropdown box on the tab.
The Trace Format hotspot to the left of a trace grid can also be used to select a trace format.
Trace formats that show trace data with a time axis:
- Log Mag (dB)
- Log Mag (lin)
- Linear Mag
- Real (I)
- Imag (Q)
- Wrap Phase
- Unwrap Phase
- Group Delay
- Q-Eye
- I-Eye
- Trellis-Eye
Trace formats that show an x-y plot of the trace data:
See Also