Setting up a New User Color Map
To define a new user color map, follow these steps:
- Open the color map editor by clicking
- Specify the (the number of colors in the map).
- Set to 0.
- Click and select the desired color for the lowest color in the color bar.
- Increase the by 1.
- Repeat the previous 2 steps until you have defined all the colors in the map.
See Also