Limit Line Editor Dialog Box (Limit Tests)
The Limit Line Editor dialog box provides the interface to create and edit limit lines. Multiple lines may be defined for a test. The limit lines are listed by name in the Limit Test Editor Dialog Box. One selected line can be edited at a time. The Limit Line Editor dialog box has three tabs, each used to define a part of a limit line.
|
Name |
A single line text box for naming or renaming a limit line. This identification is useful in editing and is displayed in the marker status box on the display.
|
|
Displays the dialog box to set the parameters of the limit line.
|
|
|
Displays the dialog box to set the units for the limit line.
|
|
|
Displays the dialog box to create and edit the limit points in the limit line. This dialog box lists all created limit points.
|
|
|
Apply |
When editing, applies any changes to the limit test on a data trace if the limit test is selected in the Limits Marker. This also automatically saves any changes made to the limit test. If a new limit test is being created, all work is saved but the limit test will not be displayed until it is selected in the Limits marker. |
See Also