Line Tab (Limit Line Editor)
The dialog box in the sets the limit line and margin properties.
The features of the dialog box are:
Test Displayed Limits check box: Enables or disables displaying the limit line. Default is selected.
Selected: Limit line appears on selected trace.
Cleared: Limit line does not appear on selected trace.
The check box must be selected in the Limits marker for a test to appear on a trace.
|
Side |
Selects an upper limit or a lower limit. An upper limit fails if the trace exceeds the limit. A lower limit fails if the trace falls below the limit.
|
|
Selects what is to be displayed: a limit, a margin, or both a limit and a margin.
|
|
|
Sets the amount of margin. This is an absolute value, the sign is ignored.
|
|
|
Determines whether the limit is one continuous line or a set of connected dots.
|
|
|
Trace Failure |
Determines whether a failure is in the trace color or a failure color. The default for this is failure color which is red for a limit line failure and yellow for a margin line failure. These can be changed in the Color Tab of the Display Preferences Dialog Box.
|
|
Apply |
When editing, applies any changes to the limit test on a data trace if the limit test is selected in the Limits Marker. This also automatically saves any changes made to the limit test. If a new limit test is being created, all work is saved but the limit test will not be displayed until it is selected in the Limits marker. |
See Also