Math Functions Reference

A math function contains an expression that is composed of data, functions, operators, and numerical constants. The output of a math function is accessed through the Trace > Data > Math submenu. You can place the math function's trace data in a trace window to view the results of the calculation.

Math Function syntax

The syntax of a Math Function Expression is similar to what you might use in C/C++ or MATLAB. Here are some examples:

Description Syntax
Statistics from Channel 2 Spectrum trace data stats(Data('Spectrum2'))
Difference of Channel 1 Time and Channel 2 Time Data('Time1') - Data('Time2')
Transfer function between channel 1 and 2 Data('Spectrum2') / Data('Spectrum1')

Also, see Creating Math Functions.

Constants (fixed)

You can select a fixed constant from the drop-down list:

π
√2
c(speed of light in m/s)

Constants (numerical)

You can use numerical constants in an expression. Here are some examples:

Real number -2
Complex number (1 + j1)
Number with exponential 3E9

Operators

There are several operators available:

x / y Divide x by y
x * y Multiply x by y
x - y Subtract y from x
x + y Add x to y
x^y x to the y exponent
-x Negate x

When x and y are vectors, the operation is performed point by point on the values in the data vectors (e.g. for multiplication, x * y = [ x[0]*y[0], x[1]*y[1], ... ]).

When x is a scalar and y is a vector, the value of x is added to each point in y.

Data

From the Data menu in the Math Functions dialog, you can select an operand to use in the math function's expression. The operand is any valid trace data or the contents of a data register. Only data registers that contain data are listed. For details about data registers, see Saving and Recalling Data Registers.

For details about any of the listed trace data, see the Trace Data book in the table of contents for the appropriate measurement type.

Trace windows are used to view a particular trace and transform the data (scaling, trace format, etc.). However, Math Functions operate on the underlying trace data vectors, so the trace data does not need to be shown in a trace window to be used in a Math Function.

The syntax to insert data into a math function Expression is as follows:

Data('dataname')

where dataname is the Data Name of the trace data or register. The Data Name is a unique identifier for a trace and does not match the trace window's title (which is formatted differently and contains other information, such as demod format). You can mouse over a trace window's title to view the tooltip, which will show the Data Name for the trace data shown in that particular trace window.

Functions

There are other functions that you can use to work with the trace data in the math expression. The following table contains information about each of the available functions:

Function Description Expected data
conj(x)

Calculate the complex conjugate of the elements in x

Re{x} - j*Im{x}

Doesn't matter
cos(x)

Calculate the cosine of the elements in x.

Doesn't matter
diff(x) Calculate the differences of adjacent elements of x. Doesn't matter
exp(x)

Compute the natural antilog of the elements in x.

The natural antilog (e^k) of a complex number k = a + jb is defined as e^(a+jb) = e^a * (cos b + j*sin b).

Doesn't matter
exp10(x)

Compute the common antilog of the elements in x.

The common antilog (10^k) of a complex number k = a + jb is defined as 10^(a+jb) = 10^a * (cos b*L10 + j*sin b*L10), where L10 is the natural log of 10.

Doesn't matter
flat(x) Apply a flat top window to the vector x. Time domain
gauss(x) Apply a gaussian window to the vector x. Time domain
hann(x) Apply a Hann window to the vector x. Time domain
fft(x)

Perform a Fast Fourier Transform of x.

Use the flat(), gauss(), or hann() function to window the time data.

Time domain
ifft(x) Perform an Inverse Fast Fourier Transform of the vector x. Frequency domain
imag(x) Compute the imaginary part of the elements in x. Doesn't matter
jw(x)

This function creates an vector of complex values equal to jω. (where ω = 2π * frequency). The frequency values to use are provided by the input vector x.

For example, say that x is a spectrum trace with center = 10 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second. and span = 5 MHz and has 801 points. Then jw(x) would contain 801 points, with value (j * 2π * 7.5 MHz) at the start of the vector through (j * 2π * 12.5 MHz) at the end of the vector.

Frequency domain
log(x) Compute the natural log (base e) of the elements in x. Doesn't matter
log10(x) Compute the common log (base 10) of the elements in x. Doesn't matter
mag(x) Compute the magnitude of the elements in x. Doesn't matter
magsq(x) Compute the magnitude squared of the elements in x. Doesn't matter
neg(x) Negate the elements of x. Doesn't matter
peak(x)

Compute the peak of the elements in x.

If the operand is complex, then the value with the maximum magnitude is calculated.

Doesn't matter
phase(x) Compute the phase of the elements in x. Doesn't matter
real(x) Compute the real part of the elements in x. Doesn't matter
sin(x)

Calculate the sin of the elements in x.

Doesn't matter
smoothing(x,y)

Smooths the response data in x using a triangular moving average filter of length y (in points).

Doesn't matter
sqrt(x) Compute the square root of the elements in x. Doesn't matter
square(x) Compute the square of the elements in x. Doesn't matter
stats(x)

Compute a table of statistics describing the data in the vector x.

See section below for more information about the contents of this table.

Doesn't matter
tan(x)

Calculate the tangent of the elements in x.

Doesn't matter
unwrap(x)

Unwrap the phase of x. This assumes the data in x is phase data.

Use unwrap(phase(data)) to compute the phase of an operand and then unwrap the phase.

Phase data
xcorr(x,y) Compute the cross-correlation between x and y. Doesn't matter
zero(x) Output is a vector, sized to match the operand, filled with zeros. Doesn't matter

Stats() table reference

When the stats() function is applied to a data vector, the following items are calculated:

All calculations work directly on the Y-axis values of the data if the trace is real-valued, or on the magnitude of the Y-axis values when the data is complex. In the table below, "Y values" means either Y or mag(Y) depending on whether the trace is real or complex.

Metric name

Description

Points

Total number of Y points in the trace.

Delta

X-axis delta between points.

Length

If the trace is NOT in the frequency domain, the value is Points * Delta. If the trace is in the frequency domain, the value is usually (Points-1)*Delta.

When Show All Frequency Points is selected, then the value may be calculated as is Points * Delta under certain conditions.

Mean

Mean of the Y values.

1/Points * sum(y[n], n = 0...Points-1)

Sum

Sum of the Y values.

sum(y[n], n = 0…Points-1)

Mean Sqrs

Mean of the magnitude squared of the Y values.

1/Points * Sum(mag(y[n])^2, n = 0...Points -1)

Sum Sqrs

Sum of the magnitude squared of the Y values.

Sum(mag(y[n])^2, n = 0…Points-1)

RMS

RMS value of the Y values.

Sqrt(Mean Sqrs)

SmSqr/ENBW

If the trace is frequency domain, this is Sum Sqrs / (ENBW * zeroPaddingRatio). Otherwise, this is just equal to Sum Sqrs.

where zeroPaddingRatio = original time-domain points / actual FFT Fast Fourier Transform: A mathematical operation performed on a time-domain signal to yield the individual spectral components that constitute the signal. See Spectrum. points

The length of the time data from which the frequency-domain trace was calculated may not have been a power of 2. In this case, the time data is zero-padded to the next power of 2 for the FFT. The zeroPaddingRatio adjusts the SmSqr/ENBW calculation to account for the frequency-domain trace having more points than the original time-domain trace.

Median

Median of the Y values.

Harm Mean

Harmonic mean of the Y values.

Points / sum(1/y[n], n = 0...Points-1)

Max

Maximum Y value.

Min

Minimum Y value.

Max Abs

Y value with maximum absolute value (for complex data, this is the same as Max, because we are operating on magnitudes already).

Min Abs

Y value with minimum absolute value (for complex data, this is the same as Min, because we are operating on magnitudes already).

InterpPeak

Interpolated peak Y value, calculated by using a quadratic fit between points, and finding the peak of the resulting waveform.

InterpPkLoc

The X-axis location of the interpolated peak Y value. This can be between the actual X-axis values of the data.

Peak/RMS

Max Y value / RMS

Slope

The slope of a line that is fit to the data. A linear regression is done to compute the line.

Intercept

The Y-axis intercept of a line that is fit to the data. A linear regression is done to compute the line.

Correlation

Correlation value from the linear regression. The value is between -1 and 1. Values with larger absolute value indicate that the linear regression line is a good approximation of the relationship between X and Y.

Std Dev

Standard deviation of the Y values. This is the estimated population standard deviation, not the sample standard deviation.

sqrt(Variance)

Variance

Variance of the Y values. This is the estimated population variance, not the sample variance.

Points/(Points - 1) * (Mean(Y^2) - Mean(Y)^2)

Skew

Skew of the Y values. Skew is a measure of whether the data has a longer tail towards the left (negative skew) or towards the right (positive skew), and is sort of a third-order equivalent of standard deviation.

Kurtosis

Kurtosis of the Y values. Kurtosis is a measure of the "spikiness" of the data, and is sort of a fourght-order equivalent of standard deviation. The kurtosis for Gaussian rand data averages to zero.

See Also

About Math Functions

Math Function Dialog Box