Search Length (802.15.4 HRP UWB)
is the amount of data to acquire and search for a HRP UWB frame. Some extra data is acquired to account for filter settling and possible trigger offset. The minimum value for Search Length is the time required if a trigger were provided that indicated the start of the frame.
There is a limit to how close to the beginning of the time capture (Raw Main Time) that the frame can be found.
is specified in units of seconds.
See Also