MMS Packet (BETA)(802.15.4 HRP UWB)
enables 802.11ab MMS (multimillisecond) packet analysis. In this mode, there is no PSDU 1) PHY Service Data Unit, or 2) PLCP SDU or PHR part of the frame, so the corresponding parameters are not visible. The MMS mode consists of SHR, any RSFs, followed by any RIFs. There can be 0-5 RSFs or RIFs. Each part of the frame is started on a millisecond boundary.
MMS Packet is available when PHY Mode is set to ERDEV HPRF and STS Packet Configuration is set to After SFD Start frame delimiter, no data (3).
Default: Disabled
See Also