Legacy Options Tab (Licenses)
The tab on the Licenses dialog box lists all features that are available under previous model/option frameworks (e.g., 89601B) for the currently installed VSA software version. See License Mappings for a comparison of 89601C features and legacy option licenses.
Code -Three-character code for the licensed feature.
Status - Current status of the feature's license.
Unknown: the license has not been checked.
Not Installed: the license is not installed.
Installed: the license is installed.
Valid: the license is installed and the license version is equal or greater than the minimum required license.
Checked Out: the license is valid and has been checked out.
Disabled: the license is disabled (or unchecked) by users using the Select License Options utility. The license will be ignored and considered as not installed without checking.
Description - Description of the licensed feature.
Location - Location of the feature's installed license. If not installed, the location field is blank.
Local: the license is installed on the local host.
<server name>: If a license is installed on the remote server, the column will show the server name.
See Also