Features Tab (Licenses)
The tab on the Licenses dialog box lists all features that are available under the 89601 "C" model framework for the currently installed VSA software version. See License Mappings for a comparison of 89601C features and legacy option licenses.
License Model - Model number of the licensed feature ("89601" + three-character feature code + "C").
Status - Current status of the feature's license.
Unknown: the license has not been checked.
Not Installed: the license is not installed.
Installed: the license is installed.
Valid: the license is installed and the license version is equal or greater than the minimum required license.
Checked Out: the license is valid and has been checked out.
Disabled: the license is disabled (or unchecked) by users using the Select License Options utility. The license will be ignored and considered as not installed without checking.
Version - Version of the license. If the version is equal or greater than the minimum required version (on the Status tab), the license is valid.
Description - Description of the licensed feature.
Location - Location of the feature's installed license. If not installed, the location field is blank.
Local: the license is installed on the local host.
<server name>: If a license is installed on the remote server, the column will show the server name.
See Also