Include Inactive Paths (LTE-Advanced)
Cleared
can be used to show information for all C-RS Cell-specific RS/Rx paths on the MIMO traces.
Selected: all C-RS/Rx paths are shown whether or not the path is present.
Cleared: only C-RS/Rx paths that that have an average C-RS power above the antenna detection threshold will be shown on the MIMO traces.
See Also