Measurement Offset (LTE-Advanced)
0 slots, 0 symbol-times
specifies the offset from the Analysis Start Boundary to the beginning of the Measurement Interval (the data sent to the demodulator) for component carrier x. is specified in slots plus symbol-times.
When performing a Cross-carrier In-band Emissions limit test, The and Measurement Interval settings should be the same for both component carriers.
See Also