Time Tab (LTE-Advanced)

Menu Path: Analysis > LTE-Advanced Demod Properties... > Time(CCx) tab where x specifies the component carrier

The Time tab of the LTE-Advanced Demod Properties dialog box lets you access the signal capture configuration parameters. You use these parameters to isolate a segment of the time record (captured input signal) for further viewing and data analysis.

At the top of this tab there is a set of buttons for selecting which component carrier to configure. The selected component carrier (x) is indicated by the green button and by the text "CCx" in the tab title.

The Time tab lets you configure these parameters (click on the parameter name for further information):

The Timing diagram at the bottom of the time tab shows the location of the Measurement Interval within the time capture. The Measurement Interval is the part of the time capture that is shown in traces and used for calculating most metrics.

The length of the time capture is primarily determined by Result Length and Analysis Start Boundary. See the Result Length topic for more information.

The image below shows the relation between the various Time tab settings and the time traces. You can click a title to navigate to the corresponding topic.

See Also

Common Tab

Decode Tab

Format Tab

Profile Tab

Advanced tab

LTE-Advanced Demod Properties Dialog Box