Analysis Start Boundary (LTE-Advanced)
Frame
Frame, Half-Frame, Subframe, Slot (uplink only)
specifies the alignment boundary of the Result Length time data. To ensure that this alignment can be achieved, the total amount of data acquired by the VSA is at least the plus the length of the alignment boundary specified by . For example, when is set to , the total acquisition is at least + 10 slots (and the data available for analysis would start at a boundary).
Once the data is located within the time capture, Measurement Offset and Measurement Interval determine what part of the data is to be analyzed. The data is shown on the Time trace. See image below for more information.
cannot be set to for downlink signals since MIMO Decoding must be applied beginning at a subframe boundary.
Since uplink signals do not contain a separate synchronization channel, the demodulator cannot determine the frame boundary exactly unless there is a unique slot in a user mapping and that unique slot is present within the Search Time data.
While most parameters can be set differently for each component carrier, this parameter is required to be the same across all component carriers.
See Also