Time Offset (LTE-Advanced)
is the offset to the Analysis Start Boundary and is expressed relative to the trigger t=0 point when Trigger Delay = 0 sec. When Trigger Delay is non-zero, then Trigger Delay will be subtracted from the Time Offset value.
The time offset will not exceed the analysis boundary period length (any integer multiple of the analysis boundary period will be subtracted from the TimeOffset).
For configurations with multiple component carriers (CC), the for each CC is calculated relative to a user-selected Reference CC and displayed as Time Alignment Error (TAE) in the Cross CC Summary trace.
See Also